Technical FAQs

Ask a Question

Is it necessary to have Lexium CT installed before installing Lexium 32 Flash Tool.

It was must to have Lexium CT installed before installing Lexium 32 Flash tool”setup_flash3_v2.5” but with newer version of Lexium 32
Flash tool” Setup_flash3_V2.7”, it is not required. Lexium 32 Flash tool”setup_flash3_v2.7” can be installed independently.
 
To install Lexium 32 Flash tool3 V2.7, refer to the link below
 
Was this helpful?
What can we do to improve the information ?