Technical FAQs

Ask a Question

With ATV312,keeps on pressing MODE button during 3 seconds, drive should switch from remote configuration to Local configuration and vice-versa but it is not working. What could be the reason.

 Remote to Local configuration switching and vice-versa by means of pressing MODE button for 3 seconds is made available
to ATV312 drive from product version v5.1 IE54. So, verify that product version of ATV312 is not older than V5.1 IE54.
Was this helpful?
What can we do to improve the information ?