Technical FAQs

Ask a Question

Error Code 127 is produced when XXMIT is used.

The XXMIT function block can only be used in MAST task.
There is an immediate fault code 127 if it is used in the FAST / AUX or EVENT tasks.
Was this helpful?
What can we do to improve the information ?