Technical FAQs

Ask a Question

What is the difference between TSXPLP01 and TSXPLP101.

TSXPLP01 and TSXPLP101 are used for Internal RAM memory backup on TSX P57 processors and fitted in the power supply module.
 
TSXPLP01 is reference for selling one battery where as TSXPLP101 is used for selling as a pack of ten TSXPLP01.
Was this helpful?
What can we do to improve the information ?