Technical FAQs

Ask a Question

How can the ATV61 drive be prevented from going into reverse when the HMI dial is turned to the negative range?

In Menu 1.6 COMMAND, set RV Inhibition to Yes.  This also applies to the ATV71 drives.
Note that this does not prevent reverse operation when the request is sent by logic input.

CTA-ID : 2062029
Was this helpful?
What can we do to improve the information ?