Technical FAQs

Ask a Question

How do I find the default IP address of an Advantys STB network interface module?

The default IP address can be determined using a tool within the Advantys configuration software;

Follow the steps below;

Select 'connection settings' from the 'Online' menu in Advantys.  



Select TCP/IP and then 'settings'.  



After clicking 'Derive IP from MAC', select the Advantys module in question from the dropdown list and enter it's mac address (this is printed underneath the ethernet port of the STB module)





The IP address is then calculated for you.



 
Was this helpful?
What can we do to improve the information ?