Technical FAQs

Ask a Question

How can ATS01N2...LU, QN, RT be started without control wires?

Add a jumper between terminals LI+ and LI2.  This provides a continuous RUN command.  When power is supplied to the ATS01, it will immediately begin to start the motor.  Removing power will result in a freewheel stop.

CTA-ID : 2062087
Was this helpful?
What can we do to improve the information ?