Technical FAQs

Ask a Question

ATS22 soft start is tripping on SnbF and this code cannot be cleared.

SnbF indicates that too many starts were attempted based on the settings for parameters Snb (number of starts) and SLG (starts period).  The soft start can be reset after the ``starts period`` has timed out.  Another option is to set parameter Snb to OFF and then cycle power to the ATS22. The fault code SnbF will clear.  Snb should then be set to the desired ``number of starts`` for the application.


CTA-ID : 2062187
Was this helpful?
What can we do to improve the information ?