Technical FAQs

Ask a Question

What is ABE7H34E100 used for.

The ABE7H34E100 is Economical kit for M340 family. It has 2 sub bases with HE10 Connectors
at one end and at other end it has 40 Pin Connector.
 
The Kit is used to connect Digital IO’s modules like BMXDDI3202K etc.
 
The Pictorial view for ABE7H34E100 is as below

Was this helpful?
What can we do to improve the information ?