Technical FAQs

Ask a Question

What are the default ports for FTP ( File Transfer Protocol ), Telnet, HTTP ( Hypertext transfer protocol ), NTP ( Network time protocol ), Modbus TCP Protocol.

The port numbers in the range from 0 to 1023 are the well-known ports. They are used by system processes that
provide widely used types of network services. The default ports are as below.
 
FTP >> Port 21
HTTP >> Port 80
Modbus TCP >> 502
NTP >> 123
Telnet >> 23
Was this helpful?
What can we do to improve the information ?