Technical FAQs

Ask a Question

What is TSX CRJMD25 Cable.

The TSX CUSB 485 converter requires the use of the TSX CRJMD 25 cable (equipped with 1 mini-DIN connector and 1 RJ45 connector).
TSX CUSB 485 + TSX CRJMD 25 cable is used to connect Premium CPU having TER port with PC loaded with Unity Pro software on
USB connectivity.

Was this helpful?
What can we do to improve the information ?