Technical FAQs

Ask a Question

Do the ATS22 Softatrts come with Modbus connection?

 Yes, the ATS22 Softstart comes with a RJ45 Modbus connector for use with Remote Terminal, SoMove Software or Communication Bus. The transmission mode used is RTU.
Was this helpful?
What can we do to improve the information ?