Technical FAQs

Ask a Question

I am not able to open more than 4 windows using super genie in Vijeo Citect.

The maximum number of windows that can be open simultaneously is 4 by default.
Using [Page]Windows ini parameter ,
You can sets the maximum number of windows supported by Vijeo Citect.

Allowable Values
: 1 to 100
Default Value: 4
You might not be able to open more number of windows, as windows could run out of system resources before you reach this limit.
Was this helpful?
What can we do to improve the information ?