Technical FAQs

Ask a Question

How can I write numeric values in a variable tag of Vijeo Citect.

Select a Numeric value ##### from the toolbar and paste it on graphics page. Then right click on it and go to properties.
Then select Input & Keyboard command tab, in key sequence type #####ENTER and in key sequence command put the
variable tag which you want to write and make it equals to “Arg1” as shown :


Was this helpful?
What can we do to improve the information ?