Technical FAQs

Ask a Question

An ATS22 display is showing OHF (Over Heating Fault), but the starter has not been run for several hours and the ambient condition is very cold.

The low end operating temperature for the ATS22 is 14 degrees F.  Below this, the starter will fault and show OHF.  OHF is an indication that the starter is outside of its operating temperature, high or low.   Heat the starter until it is above 14 degrees F and the display should change to normal status, rdY or nrdY.   If this happens often, consider some type of heater that can turn on when the temperature falls below freezing to keep the starter within its usable temperature range.

CTA-ID : 2062514
Was this helpful?
What can we do to improve the information ?