Technical FAQs

Ask a Question

ATS01: What happens if a new start command is given soon after a stop command when using ramp down function?

If a new start command is given before the motor stops, the motor will start again immediately. It does not wait for the motor to stop.  For the ATS01, any run order is taken into account to start the motor as soon as it is given to the soft starter.

CTA-ID : 2061902
Was this helpful?
What can we do to improve the information ?