Technical FAQs

Ask a Question

In Ecodial Advance Calculation, how to resize a busbar or a busbar trunking?

• Select the busbar (The object is highlighted with “Green” colour)
• Place the cursor nearer to the end of the busbar, at which the resizing is required.
• The double headed arrow will appear, then click and hold to resize the busbar. The increase in size takes place in steps, so do not hesitate to significantly enlarge the busbars.

 

 

 
 

Was this helpful?
What can we do to improve the information ?