Technical FAQs

Ask a Question

In Ecodial Advance Calculation, Is there any limit in connecting number of circuits in the network?

In Ecodial Advance Calculation, There is no limit in connecting “number of circuits” on a network.

(But, please consider the maximum rating of the transformer available in Ecodial for the selection. If the network is supplied by a "single" HV/LV transformer, then it can only be loaded up to the available maximum rating of the transformer & it limits the user in connecting number of circuits on the network)
 

Was this helpful?
What can we do to improve the information ?