Technical FAQs

Ask a Question

What is the ATS22 adjustable range for ILt, current limit?

The range is 200% to 700% of parameter In, motor rated current.  The maximum is limited to 350% of the ATS22 amp rating.
If the application requires more than 350% of ATS22 rating, then the soft starter must be upsized.

CTA-ID : 2062727
Was this helpful?
What can we do to improve the information ?