Technical FAQs

Ask a Question

In Ecodial Advance Calculation, Is it possible export the schematic in an AutoCAD format?

YES, the project (schematic / line diagram) created by the Ecodial Advance calculation, can be saved or exported in AutoCAD format.

 
On the “Tool Bar”, there is an icon with the letter “Dxf”…

Clicking this icon / button will lead to save/export the “on screen diagram” in the .Dxf format.
.Dxf is the AutoCAD compatible format.

Was this helpful?
What can we do to improve the information ?