Technical FAQs

Ask a Question

In Ecodial Advance Calculation, will it possible to create a network with Generator as a source?

YES, In Ecodial Advance Calculation – It will be possible to create & design a network with generator as a source.

[This question is due to the following behaviour of My Ecodial L]

In My Ecodial L, if the user try to calculate the network with only Generator source. then My Ecodial L will raise an alarm stating that, there is no main source present in the network. It’s because, My Ecodial L always considers the generator as a “Replacement Source”. But still in My Ecodial L user will be able to calculate the network having only generator, stating that generator is the “main source” of the network. (On the ‘Circuit description’ - remove the check mark from the characteristics – Replacement source)


Was this helpful?
What can we do to improve the information ?