Technical FAQs

Ask a Question

In Ecodial Advance Calculation, how will I do the worksheet selection?

YES, sometimes it is better to pre select the work sheet – before start design the schematic.

 
To do the worksheet selection,

• From the “Tool Bar” click the “Print” icon…a drop down menu will appear.

• From the ‘drop down’ menu, select the “Page setting”. 

• From the “Page setting” window, select the “paper size” & “Layout” then click OK to implement the selection.

 
 

Was this helpful?
What can we do to improve the information ?