Technical FAQs

Ask a Question

In Ecodial Advance Calculation, how do I determine the printable area?

On the TAB “Design and Sizing”, there is an icon     to show the ‘printing borders’ over the diagram.
Before clicking this   icon,
If the user has already done the “worksheet selection” & “layout settings” with the help of “page setting”, then Ecodial will place the ‘schematic’ in the selected worksheet(s)

 
(From the above image), we cans see the printable area determined by the software
 

Was this helpful?
What can we do to improve the information ?