Technical FAQs

Ask a Question

In Ecodial Advance Calculation, the cable component has a button called "Hide the link", what is the use of it?

At any circuit, the component below the ‘cable component’ can be moved for a distance (diagrammatically) from its actual presence.

In this case, the electrical link between the cable component & the next component can be “displayed or hidden” by using this button.

(Click the button to “Hide the link”)                                       (Click the button to “Display the link”)


Was this helpful?
What can we do to improve the information ?