Technical FAQs

Ask a Question

In Ecodial Advance calculation, how to create the "operating modes"?

By default, the design and sizing of an electrical schematic starts with the “Normal” Operating mode’.

 

If the designer is interested to create more operating conditions then, He should use the function “Management of operating modes”

 

From the ‘drop down’ menu, Click and select the “Management of operating modes”, then a window appear and help the designer to create the other operating modes.

 

Normally the designer can “Duplicate the normal mode” and starts name them as other operating modes.

 

Was this helpful?
What can we do to improve the information ?