Technical FAQs

Ask a Question

In Ecodial Advance calculation, what do you mean by "Context-sensitive help"?

 

Ecodial Advance Calculation has a “Help file”, which is well integrated with the software graphical user interface.

In all the circuits, some of the component characteristics have a ‘help icon’ associated with it.

If the user clicks the help icon, nearer to the component characteristics, then the relevant page of help file will open for the user.
These help icons are normally called as the “context sensitive help”

Once user verified the relevant subject, it’s better to close the help file.
If the user keeps open help file, then the consecutive trails for the “context sensitive help” will not take him to the relevant subject. Because this is the property of Adobe Acrobat file to "set & reach" the file destinations.

 

Was this helpful?
What can we do to improve the information ?