Technical FAQs

Ask a Question

In Ecodial Advance calculation, will it possible to draw an independent network(s) on a project?

YES, In Ecodial Advance calculation – it’s allowed to “design and size” the independent networks on a single project.
(Note: At this situation, if the user comes back and does any changes in the ‘project parameters’, it will be applicable for all these independent networks of the project.)
Was this helpful?
What can we do to improve the information ?