Technical FAQs

Ask a Question

In Ecodial Advance Calculation, will it possible to define the 'general information' of project?

Yes, In Ecodial Advance Calculation the ‘general information’ of the project cab be defined. Then this can also be printed & given along with the schematic design.

On the “Tool Bar”, there is an icon for settings   Clicking this icon will open a window to set the following project information.

TAB: “Front Page” is to know the information about the user
TAB: “Company” is to know the information about the users company
TAB: ”Project” is to know about the project

Was this helpful?
What can we do to improve the information ?