Technical FAQs

Ask a Question

In Ecodial Advance Calculation, why the 'number and type of conductor' is always "undefined" for the Feeder circuit?

In Ecodial Advance Calculation, value for this parameter ‘number and type of conductor’ will be propagated from down-to-top basis.

At the switchboard level, if we connect different types of loads (1Ph+N, 2Ph, 3Ph, 3Ph+N) , then we can verify this parameter ‘number and type of conductor’ for different values. 
Based on the type of load connected, we can see the value propagated at the switch board level.
 

Was this helpful?
What can we do to improve the information ?