Technical FAQs

Ask a Question

In Ecodial Advance Calculation, will it possible to make the constraint cascading as an optional for protection selection?

YES, In Ecodial Advance Calculation – the “Cascading” constraint is optional for the protection device selection.
In any circuit block, if the selected the protection device type is ‘circuit breaker’ then the user will find the option to set the ‘cascading’ constraint.
It is user’s choice is to consider the cascading as constraint for protection device selection or not.

(The above image shows the ‘cascading constraint’ is not considered by selecting the value ‘No’)

Was this helpful?
What can we do to improve the information ?