Technical FAQs

Ask a Question

What are the selection criteria’s followed by Ecodial Advance Calculation, to determine the "type of LV capacitor banks”?

LV capacitor banks are available for 3 levels of harmonic withstand:

- Gh/Sn < 15%, "Classic" capacitor banks can be used

- 15% ≤ Gh/Sn < 25 %, the capacitor banks must be at least of the "Comfort" type (the "Classic" type is not allowed)

- Gh/Sn ≥ 25%, "Harmony" capacitor banks must be used (the "Classic" and "Comfort" types are not allowed).

If Gh/Sn exceeds 50%, a special study must be carried out to determine the type of capacitor bank because harmonic filtering must be installed.

Was this helpful?
What can we do to improve the information ?