Technical FAQs

Ask a Question

What is the benefit of Evacuation function on Altivar 71 drive.

This function is suitable for lift application, when there is a power failure; it facilitates the evacuation
of people trapped in a lift stuck between two floors.
This can be used to control the reduced speed engine with
a reduced voltage supply (220 V , for example: uninterruptible power supply (UPS)),by preserving torque performance.
Was this helpful?
What can we do to improve the information ?