Technical FAQs

Ask a Question

What is the maximum operating temperature & IP of the Remote graphic display terminal of the Altivar 71 Drive.

The maximum operating temperature of the Remote graphic display terminal is 60°C and it has IP 54 Protection.
Was this helpful?
What can we do to improve the information ?