Technical FAQs

Ask a Question

While installing OFS software from VJC installation files , it was asking for Serial Number & part reference.

If you run the OFS installations directly from the installation files then it will ask for Serial Number and Part
number, but to install it directly you have to start installation from the launch.exe and then select OPC Factory
Server then it will automatically fill the serial details.
Was this helpful?
What can we do to improve the information ?