Technical FAQs

Ask a Question

What is the difference between Vijeo Citect Unity Speedlink Dynamic and Unity Speedlink Static.

Vijeo Citect Unity Speedlink Dynamic is a tool used for linking to a Unity Pro *.stu file project file. It makes a dynamic
link between Vijeo Citect and the Unity project so that variables update occur at Vijeo Citect side automatically from
linked Unity project file.
Unity Speedlink Static tool is used for linking with a Unity *.xsy file. It makes a static link between
Vijeo Citect and Unity project so variable related updates has to be refreshed manually.
Was this helpful?
What can we do to improve the information ?