Technical FAQs

Ask a Question

How can I make VJC as a OPC Client to get data from an OPC Server.

For communicating VJC with an OPC Server, you have to select OPC in the IO Device configuration. When you run IO Express Wizard, you
have to select OPC Foundation as shown in below snap then it will import tags from the selected OPC Server automatically.



Was this helpful?
What can we do to improve the information ?