Technical FAQs

Ask a Question

Is it possible to connect a 3 Pole Compact NSX breaker to use for single phase application.

If you need to protect a single phase with a NSX in 3P you can connect the load (phase 1) to the pole 1 and
the load (neutral) to the pole 3. Pole 2 of the breaker not connected.
Was this helpful?
What can we do to improve the information ?