Technical FAQs

Ask a Question

Can the ATS48 run in a test mode when a motor is not connected?

Issue:
Can the ATS48 run in a test mode when a motor is not connected?

Product Line:
Altistart 48 ATS48

Environment:
All models

Cause:
Does ATS48 have same ability as a VFD to run with motor disconnected?

Resolution:
No.  The unit must have output current or it will fault on PHF.  For testing purposes, setting menu drC, parameter SSt = ON allows the use of a small motor compared to the ATS48 rating.  Note that SSt does have limits for very small currents and may trip PHF.
Was this helpful?
What can we do to improve the information ?