Technical FAQs

Ask a Question

What is the use of Automatic adaptation of deceleration ramp parameter on Altivar 312 drive.

This function is used to automatically adapt the deceleration ramp if the initial setting is too low for the inertia of the load connected.
It avoids the drive locking in the event of an overbraking fault.
The function is suitable for all applications which do require precise s
topping and do not use braking resistors.
Automatic adaptation must be cancelled if the machine has position control with stopping on a ramp and a braking resistor installed.
It is automatically disabled if the brake sequence is configured.
Was this helpful?
What can we do to improve the information ?