Technical FAQs

Ask a Question

How we can run Altivar 312 drive without motor load.

Configure following parameter 

FLt (Fault menu) OPL (Output phase loss)= NO. 
By setting above parameter, you can check drive without physical connection of motor.
Drive will follow frequency reference and control (Start/ Stop) command and will not trip on “Output phase loss”.
Was this helpful?
What can we do to improve the information ?