Technical FAQs

Ask a Question

We frequently need to view the Trends from the trends backup files inside the Vijeo Citect project. The backup files are the trends files moved from the trend folder into a backup folder.

To view trend data in Vijeo Citect runtime, you need to add the trend files in Citect with help of the " TrnAddHistory " function available .
 Details of this function attached below.
Was this helpful?
What can we do to improve the information ?