Technical FAQs

Ask a Question

Report using Report Development Tool of VJH 4.3 ,The report looks fine when viewed on any of the browsers, but when we use ‘export to PDF’ option, the appearance of the report gets changed.

You need to change the Page Size of the report in Format report . Change the report Width, height will be automatically adjusted
according to the report length. You have to make changes such that it will suits the PDF format ,
when you create report in design mode , you can see a horizontal scale at the top remember paper size is 6 inches in width and 11 inches in length 
you need to keep it in mind and design ur report, if u drag the report size beyond 6 inched ur columns will appear on next page only.
Was this helpful?
What can we do to improve the information ?