Technical FAQs

Ask a Question

How can I configure Menu in the tab style template.

Page menus in the tab style templates are defined using the Menu Configuration dialog. For tab templates the fields have the following properties:
Order
The relative display position of the tabs / buttons or menu items among themselves. For the tabs and buttons, it determines the display order
from left to right. For the drop-down menu items, it determines the display order from the top to the bottom. If this field is left blank, it will take the
default value of 0. The relevant entries will be displayed at the start as a result. If more than 1 entry of the same order exists, they are displayed
in the same order as they are defined in the database.
Level 1
This represents the tabs on the tab bar.
Level 2
This represents the buttons displayed under a particular tab.
Level 3
This represents the menu items of the dropdown menu next to a particular button.
Level 4
This represents the sub-menu items of a particular dropdown menu item.
Menu Command
The Cicode expression to be executed when the menu item is selected. String of 256 characters.
Symbol
The symbol to associate with the menu entry in the format of <library name>.<symbol name>. The template expects the symbol to be a certain size
when it is configured against different menu types: For tabs, symbols are 16 x 16 pixels. For buttons, symbols are 32 x 32 pixels. Some common
symbols can be found in the symbol libraries of icons_16x16 and icons_32x32. The field is not applicable for menu and sub-menu items.
Comment
A comment about the menu entry. String of 128 characters.
Was this helpful?
What can we do to improve the information ?