Technical FAQs

Ask a Question

How can I change a INI parameter during Citect Runtime.

You can update a INI parameter with help of the function “ParameterPut”. This function updates a system parameter in the CITECT.INI file.
If the system parameter does not exist, it is added to the CITECT.INI file.
ParameterPut(Section, Name, Value)
The section name.
The system parameter name.
The value to put in the system parameter.
Return Value
0 (zero) if successful, otherwise an error is returned.
Was this helpful?
What can we do to improve the information ?