Technical FAQs

Ask a Question

What are the pinouts for the Micrologic trip unit Breaker communication module (BCM)?


Issue:
BCM wiring

Product Line:
Circuit Protection:

Environment:
Electrical Distribution Equipment

Cause:
How to wire BCM on Powerpact P, R and Masterpact NW and NT.

Resolution:

From left to right:

E1: 24Vdc
E2:  GND
E3: Out-  Black
E4 Out+  Red
E5: In-   White
E6: In+  Green


CTA-ID : 2063020
Was this helpful?
What can we do to improve the information ?