Technical FAQs

Ask a Question

What is the memory capacity of the processor used on the Micrologic 5 or 6 E trip units.

The microcontroller has 512 Kbytes in Flash memory and 32 kBytes in RAM on the Micrologic 5 or 6 trip units.
Was this helpful?
What can we do to improve the information ?