Technical FAQs

Ask a Question

Is there any dual redundancy available with TeSys T’s offer.

Yes, it is available with Ethernet Product only. This is the dual port technology which allows that.
The redundancy is for Ethernet Communication Port for the TeSys T but not for the CPU into the product.
There is only one CPU into TeSys T.
Was this helpful?
What can we do to improve the information ?