Technical FAQs

Ask a Question

What is the limit on Modbus multi drop connection for both the HMI port and also on the Modbus port in TeSys T.

The limit on the left or the right port for TeSys T Modbus product is the same.
These features are defined by Modbus standard: maximum 1000 meters without repeater and 31 maximum slaves.
Was this helpful?
What can we do to improve the information ?