Technical FAQs

Ask a Question

What is the default baud rate , address and parity of Breaker Communications Module (BCM) and Chassis Communications Module (CCM).

For the CCM the Default values are: Baud rate = 19.2 K , Address = 97, Parity = even
For the BCM the default values are: Baud rate = 19.2 K,  Address = 47, Parity = even
Was this helpful?
What can we do to improve the information ?