Technical FAQs

Ask a Question

Does the Modbus Chassis Communication Module (CCM) support 2 wire RS485 communications.

The Modbus Chassis Communications Module does support 2 wire RS485 communications.
The module can be configured by jumpering the IN+ and the OUT+ and the IN- and the OUT-.
Was this helpful?
What can we do to improve the information ?